FOR IMMEDIATE RELEASE No. 2992

Mitsubishi Electric Develops High-precision Air-quality Sensor for PM2.5

World's first air quality sensor can distinguish PM2.5, pollen and dust

PDF Version

TOKYO, February 8, 2016 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has developed a small, high-precision air-quality sensor, the world first to detect all fine particles measuring no more than 2.5 micrometers in diameter, called PM2.5, as well as pollen and dust. It also senses the density of particles precisely.

Prototype of Mitsubishi Electric's new air-quality sensor

Prototype of Mitsubishi Electric's new air-quality sensor

Scattered light from PM2.5 particles is measured with Mitsubishi Electric's unique double-sided mirror design, which collects about 1.8 times more scattered light than conventional single-sided designs. An air flow controller provides stable airflow. Components were optimally designed to achieve a small form factor and were carefully aligned to avoid obstructing the airflow and laser beams. Mitsubishi Electric's original shape-discrimination algorithm distinguishes between pollen and dust based on the respective differences in the optical characteristics of their scattered light, resulting in the world's first sensor capable of detecting all PM2.5, pollen and dust particles.

The air-quality sensor prototype consists of a laser diode, aspheric lens, light-collecting mirror, photodetector and airflow controller. The prototype measures 67mm (W) x 49mm (D) x 35mm (H). The minimum size of a detectable particle is just 0.3 micrometer.

PM2.5 has posed a serious problem, causing air pollution and health-related issues in countries such as China, India and Japan. The trend has raised public concerns and increased the demand for high-precision air-quality sensors to detect PM2.5. At present, however, high-precision sensors for PM2.5 are large and expensive, limiting their applications to commercial use only.

Note that the releases are accurate at the time of publication but may be subject to change without notice.