With over 100 years of experience Mitsubishi Electric is a world leading company in providing high reliability solutions. For energy efficiency and safety solutions, the company provides a complete offer, with different levels of solutions capable of responding to the different needs of customers and allows the creation of systems for each type of application. In addition, Mitsubishi Electric offers a global support service thanks to the widespread presence of support centres all around the world.

Dive into our solutions

EM-A with FR-E800

EM-A Series include newly developed magnetic motors using the patented salient-pole core. The rotor consists of the salient-pole core and surface-mounted permanent magnet, and therefore the motor inductance changes depending on the rotational position. This change in inductance is applied to the sensorless control. The combination of the newly developed salient-pole magnetic motor and Mitsubishi’s unique high-performance sensorless control technique realizes high precision speed control and positioning control without a sensor (encoder).

Download our catalogue here!
Select...

By filling in this form, you consent to the data entered being processed by the company MITSUBISHI ELECTRIC EUROPE BV and / or its subcontractors, as data controller for the purposes of the organization and implementation of the training in question. Participants benefit from a right of access, rectification, erasure (right to be forgotten), limitation of processing, opposition and portability of personal data concerning them. In the event that participants wish to exercise any of these rights, they must make a request to MITSUBISHI ELECTRIC EUROPE B.V. by email to the following address: LDPC.France@fra.mee.com. Our privacy policy is accessible via the following link: fr.mitsubishielectric.com/fa//en/privacy

The fields marked by a * are mandatory.

Inverters | FREQROL

Mitsubishi inverters are real energy savers achieving maximum drive capacity utilisation with minimum power consumption. Flux optimisation ensures that the connected motor only gets exactly the amount of magnetic flux required for optimum efficiency. They can achieve maximum power savings of up to 60% compared to conventional mains operation, thus minimising system operating costs.

Take a look at our videos

Discover our whitepaper!

Click on the image to download our whitepapers

Digital Wave in Water Treatment

“Water is the driving force of all nature” is a quotation from Leonardoda Vinci. Water is also a vital resource in the economic development, theagriculture, all sectors of industry and the sustainability of communities.We should therefore do everything possible to conserve our waterresources. Discover how new technologies facilitate this.

Get More Value from your VFD

In a world where motors power critical systems across industries, variable frequency drives (VFDs) have become an essential component for success. Modern VFDs are smarter, more compact, more powerful, more energy efficient, and have a wealth of advanced capabilities that organizations might not be taking advantage of.

Advances in Motor Technology and Energy Efficiency

Factories and machine builders are seeking ways to boost motor efficiency to intelligently maximize energy savings. At the same time, these users are transitioning from induction motors to interior permanent motors (IPM). These trends are propelling the need for higher performance drives that are facilitated through such innovations as variable frequency inverter technology.

Où nous trouver ?

MITSUBISHI ELECTRIC EUROPE B.V.

2, Rue de l’Union
92565 Rueil-Malmaison Cedex

Tel.: +33 (0)1 55 68 57 01
automatismes@mitsubishielectric.fr